Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

User21298
Level 1
Level 1
Hello, I posses a ecu with has two Aurix microcontrollers on it. I am connected remotely to it and I want to debug one at a time and have the other free running then. Im connecting via DAP. Basically is it possible to connect 2, is the protocol supporting this and where would I find further information how to do the cabling?
If this is not forseen, would it make sense to build up a switchbox that does the connection and what lines can be keept unswitched eg clock?
thank you very very much
7 Replies
User21298
Level 1
Level 1
hello is this question so hard or am i in the wrong forums? any hint is helpful for me. thank you!!
0 Likes
User21298
Level 1
Level 1
up n
0 Likes
User21298
Level 1
Level 1
up please macke it sticky
0 Likes
User21298
Level 1
Level 1
up ip
0 Likes
User21298
Level 1
Level 1
upupup








piup
0 Likes
User22610
Level 1
Level 1
UP! Hope you find the answer to this. I am curious about it myself
tile roofs bradenton
0 Likes
User22639
Level 1
Level 1
Please note that Carpet Cleaning Fort Mcmurray so far has the highest rating.
0 Likes