Compatibility between boards

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
AlNa_4545466
Level 1
Level 1
First question asked

I have just purchased your development kit FM4-176L-S6E2GM (1)

But it seems it was a mistake on my side as I would like to buy the similar one FME-176L-S6E2CC-ETH   (2).

This is because I want to use some code already prepared from a book for DSP applications. And the code is target for the board (2)

The problem is that it seems there is not exactly complete compatibility. When I run the code I have installed from your site my board (1) works ok. But If I run the code from the book for board (2) it seems it does not work properly.

In Keil for example I can not see the debug working properly (step by step).

Could you tell me if there are compatibility issues between the two boards.

I do not want to buy another board.

Thank you for the help.

Alberto Nascimento

0 Likes
1 Solution
ShipingW_81
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

The two boards are not exactly same. The main controllers have different core frequency, flash/sram space size, number of GPIOs.

You need adjust you code according to the hardware differences.

In addition, is it possible to exchange the boards from you purchase channel?

View solution in original post

0 Likes
1 Reply
ShipingW_81
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

The two boards are not exactly same. The main controllers have different core frequency, flash/sram space size, number of GPIOs.

You need adjust you code according to the hardware differences.

In addition, is it possible to exchange the boards from you purchase channel?

0 Likes