Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
noha_3407421
Level 3
Level 3
Distributor - TED (Japan)
First like received 10 replies posted 10 questions asked

[Device]

MB9BF568RPMC

[Backgrounds]

- Hardware transfer is performed by DSTC.

- Selecting "transfer mode1".

A "DES open error" has occurred during DSTC transfer.

-> I have confirmed that the value of EST[2:0] in the MONERS register is "101".

We confirmed the DES open error occurrence conditions described in “DES Open Error” on page 527 of “32-Bit Microcontroller FM4 Family Peripheral Manual”.

However, the values of DES0 and DES1 do not meet any of the following conditions.

================================================================

- DV[1:0]==00

- PCHK[3:0] != (DES0[27:24] ^ DES0[23:20] ^ DES0[19:16] ^ DES0[15:12] ^ DES0[11:8] ^ DES0[7:4])

- One of the two bits of the reserved area of DES0 is 1.

- TW[1:0]==11

- CHRS[5:4]==11

- (CHRS[5]==0) &&(CHRS[3]==0)&&(CHRS[1]==0) &&(CHLK ==1)

- (MODE==1)&&(IIN!=0x00)&&(IRM==0x00)

- (MODE==1)&&(IIN!=0x00)&&(IRM>IIN)

- (MODE==1)&&(DV[1]==1)&&(ORL[0]==0)&& (ORM != 0x0001)

- (MODE==1)&&(DV[1]==1)&&(ORL[0]==0) && (IRM != 0x01)

- (MODE==1)&&(DV[1]==1)&&(ORL[0]==0)&& (IIN != 0x01)

- (DV[1]==1)&&(SAC[0]==0)&&(ORL[1]==0)

- (DV[1]==1)&&(DAC[0]==0)&&(ORL[2]==0)

================================================================

Q1.

Are there any other conditions that cause a “DES open error” other than the above values for DES0 and DES1?

Q2.

The DSTC HW transfer uses 3channels.

The frequency of DES open errors increased when three input edge detection interrupts occurred simultaneously.

Is there a case where the arbitration operation does not function normally?

If so, would you tell me the workaround if there is one?

*I am referring to “3.2.5 Arbitration of Transfer Requests” on page 524 of “32-Bit Microcontroller FM4 Family Peripheral Manual”.

Best Regards,

Harukawa

--- 以下、日本語 ---

■デバイス

MB9BF568RPMC

■問合せ内容

*背景

・DSTCでhardware転送を行っています。(3チャネルを使用しています)

・転送モード1を選択しています

DSTC転送中に「DESオープンエラー」が発生しています。

-> MONERSレジスタのEST[2:0]の値が"101"になっていることを確認しています。

「32-Bit Microcontroller FM4 Family Peripheral Manual」のP527の「DES Open Error」に記載されているDESオープンエラー発生条件を確認しました。

しかし、DES0とDES1の値は下記の条件のいずれにも合致していません。

================================================================

- DV[1:0]==00

- PCHK[3:0] != (DES0[27:24] ^ DES0[23:20] ^ DES0[19:16] ^ DES0[15:12] ^ DES0[11:8] ^ DES0[7:4])

- One of the two bits of the reserved area of DES0 is 1.

- TW[1:0]==11

- CHRS[5:4]==11

- (CHRS[5]==0) &&(CHRS[3]==0)&&(CHRS[1]==0) &&(CHLK ==1)

- (MODE==1)&&(IIN!=0x00)&&(IRM==0x00)

- (MODE==1)&&(IIN!=0x00)&&(IRM>IIN)

- (MODE==1)&&(DV[1]==1)&&(ORL[0]==0)&& (ORM != 0x0001)

- (MODE==1)&&(DV[1]==1)&&(ORL[0]==0) && (IRM != 0x01)

- (MODE==1)&&(DV[1]==1)&&(ORL[0]==0)&& (IIN != 0x01)

- (DV[1]==1)&&(SAC[0]==0)&&(ORL[1]==0)

- (DV[1]==1)&&(DAC[0]==0)&&(ORL[2]==0)

================================================================

Q1.

DES0,DES1の上記の値以外に「DESオープンエラー」が発生する条件はあるのでしょうか。

Q2.

DSTCのHW転送では3チャネルを使用しています。

入力エッジ検出割込みが3つ同時に起きると、DESオープンエラーの発生頻度が上がりました。

調停動作が正常機能しない事例があるのでしょうか。

もしあるならその回避策を教えてくれませんか。

*「32-Bit Microcontroller FM4 Family Peripheral Manual」のP524の「3.2.5 Arbitration of Transfer Requests」を参照しています。

0 Likes
1 Solution
noha_3407421
Level 3
Level 3
Distributor - TED (Japan)
First like received 10 replies posted 10 questions asked

A customer survey revealed that the customer's program overwrote the DSTC transfer settings.

The "DES Open Error" could be avoided by modifying the customer program.

It turned out that there was a cause in the customer's usage.

Please close this query.

Best Regards,

Harukawa

View solution in original post

0 Likes
2 Replies
noha_3407421
Level 3
Level 3
Distributor - TED (Japan)
First like received 10 replies posted 10 questions asked

A customer survey revealed that the customer's program overwrote the DSTC transfer settings.

The "DES Open Error" could be avoided by modifying the customer program.

It turned out that there was a cause in the customer's usage.

Please close this query.

Best Regards,

Harukawa

0 Likes

Dear Harukawa-san,

Thank you very much for your update for this thread.

will lock this thread based on you comments.

if you need further support, please let us know.

thank you.

0 Likes