请问,DAP miniwiggler 连接不上xc2365A芯片?

公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
TitanS
Level 1
Level 1
First solution authored First reply posted First question asked

请问,DAP miniwiggler 连接不上xc2365A芯片?

f1d4c6ae-4688-4fe9-80f9-2b28df98fbdc.jpg

尝试过JTAG或DAP,都连接不上芯片,请问下有可能什么原因导致的。

另外,针对XC2365A的话,

1.使用JTAG的引脚是哪些,从手册中看到好多组jtag的引脚(TDI/TDO/TMS/TCK)?

2.使用DAP的引脚是哪些?

 

 

0 点赞
1 解答
TitanS
Level 1
Level 1
First solution authored First reply posted First question asked

Thanks.The reason is that P10 pin is not configured.

在原帖中查看解决方案

0 点赞
2 回复数
zzz_3221081
Level 5
Level 5
25 solutions authored 100 sign-ins 10 likes received

I think you need to refer to the datasheet of your device.

We are using a XC2286, and I can show the respective document section for this device:

zzz_3221081_0-1670310893226.png


Furthermore, DAP and JTAG seem alternative modes for the debug interface. Detection is done at startup via input lines. The datasheet says:
3.7 On-Chip Debug Support (OCDS)
...
The OCDS is controlled by an external debugging device via the debug interface. This
either consists of the 2-pin Device Access Port (DAP) or of the JTAG port conforming to
IEEE-1149. The debug interface can be completed with an optional break interface.
...
The DAP interface uses two interface signals, the JTAG interface uses four interface
signals, to communicate with external circuitry. The debug interface can be amended
with two optional break lines.

I assume the XC2365 is similiar in this regard.

 

TitanS
Level 1
Level 1
First solution authored First reply posted First question asked

Thanks.The reason is that P10 pin is not configured.

0 点赞