Microcontrollers Forum Discussions
Browse the Community
PSoC™ 6
Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.
PSoC™ 4
PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
PSoC™ 5, 3 & 1
The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.
CAPSENSE™ & MagSense
The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.
XMC™
AURIX™
In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs
TRAVEO™ T2G
Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.
MOTIX™ MCU
The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!
Legacy microcontrollers
Featured Discussions
text.format{('custom.tabs.no.results')}
Hello,
I'm running MTB 3.2 GUI in Ubuntu 22.04.4 LTS and building the Security_App PSoC6 example for the Prototyping Kit (CY8CPROTO-062-4343W).
After creating the default Security_App example, I added the emeeprom (v2.20.0) component, so as to read/write settings to the PSoC6 32kB Auxilliary Flash. I copied the code from Emeeprom's README.md
And added a line CY_SECTION(".cy_em_eeprom") , so that emEepromStorage will be kept in the 32kB Auxilliary Flash.
However, the code failed to compile:
/opt/Tools/ModusToolbox/tools_3.2/cymcuelftool-1.0/bin/cymcuelftool --merge ../proj_cm0p/build/APP_CY8CPROTO-062-4343W/Debug/proj_cm0p.elf ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/proj_cm4.elf --output ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app.elf --hex ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app.hex; cp -f ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app.hex ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app_BOOT_raw.hex; rm -f ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app.hex; /opt/Tools/ModusToolbox/tools_3.2/gcc/bin/arm-none-eabi-objcopy --change-addresses=0 -O ihex ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app.elf ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app_BOOT_unsigned.hex; ../../mtb_shared/core-make/release-v3.3.1/make/scripts/python3.bash ../../mtb_shared/mcuboot/v1.8.1-cypress/scripts/imgtool.py sign --header-size 0x400 --pad-header --align 8 -v 1.0.0 -S 917504 -M 1792 --overwrite-only -R 0 -k ../proj_btldr_cm0p/keys/cypress-test-ec-p256.pem ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app_BOOT_unsigned.hex ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app.hex; cp -f ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app.hex ./build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app_BOOT.hex;
No ELF section .cychecksum found, creating one
Application checksum calculated and stored in ELF section .cychecksum
No ELF section .cymeta found, creating one
Checksum calculated and stored in ELF section .cymeta
Usage: imgtool.py sign [OPTIONS] INFILE OUTFILE
Try 'imgtool.py sign -h' for help.
Error: Image size (0x3fe0896) + trailer (0x20) exceeds requested size 0xe0000
make[1]: Leaving directory '/home/ub2204/work/psoc/tansiowk_mtw_3_1/Security_App_Emeeprom/proj_cm4'
cp: cannot stat './build/BOOT/APP_CY8CPROTO-062-4343W/Debug/primary_app.hex': No such file or directory
make[2]: *** [../../mtb_shared/core-make/release-v3.3.1/make/core/bwc.mk:161: _mtb_build__legacy_project_postbuild] Error 1
make[1]: *** [../../mtb_shared/core-make/release-v3.3.1/make/core/main.mk:385: secondstage_build] Error 2
make: *** [/opt/Tools/ModusToolbox/tools_3.2/make/application.mk:72: build] Error 2
"/opt/Tools/ModusToolbox/tools_3.2/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_IDE_TOOLS_DIR=/opt/Tools/ModusToolbox/tools_3.2 CY_IDE_BT_TOOLS_DIR= -j6 all" terminated with exit code 2. Build might be incomplete.
I have attached the code, build error log and map file.
Thanks for any advice!
BR,
SK
Show Less你好!
在NORMAL状态下,我用WriteRow写NAR时报0xF00000AA(Writes are disabled in safety register)错误,
请问是什么原因?另外,可否提供使用WriteRow的例程?谢谢!
补充一点:这部分代码我是放在CM4里的,这可以吗?
Show LessHello,
I am trying to flash littlefs filesystem on the qspi external serial flash memory in XMC7100 V1.1. As I see library mtb-littlefs is not included in the XMC7100 kit but i have included the mtb-littlefs from PSoc6 Kit to my project and in makefile included target as XMC7100 (my board).
BOARD: XMC7100 EVK Lite v1.1
Memory: External QSPI flash memory
These are the errors when I try to builld the file:
Initializing build: mtb-example-psoc6-filesystem-littlefs-freertos Debug APP_KIT_XMC71_EVK_LITE_V1 GCC_ARM
Prebuild operations complete
Auto-discovery in progress...
Auto-discovery complete
Commencing build operations...
Tools Directory: C:/Users/Prasad/ModusToolbox/tools_3.2
"Using linker bsps/TARGET_APP_KIT_XMC71_EVK_LITE_V1/COMPONENT_/TOOLCHAIN_GCC_ARM/linker.ld"
Constructing build rules...
Build rules construction complete
==============================================================================
= Building application =
==============================================================================
Generating compilation database file...
-> ./build/compile_commands.json
Compilation database file generation complete
Building 223 file(s)
Compiling ../mtb_shared/mtb-littlefs/latest-v2.X/source/lfs_qspi_memslot.c -DCOMPONENT_APP_KIT_XMC71_EVK_LITE_V1 -DCOMPONENT_CAT1 -DCOMPONENT_CAT1C -DCOMPONENT_CAT1C4M -DCOMPONENT_CM7 -DCOMPONENT_CM7_0 -DCOMPONENT_Debug -DCOMPONENT_FREERTOS -DCOMPONENT_GCC_ARM -DCOMPONENT_MW_ABSTRACTION_RTOS -DCOMPONENT_MW_CAT1CM0P -DCOMPONENT_MW_CLIB_SUPPORT -DCOMPONENT_MW_CMSIS -DCOMPONENT_MW_CORE_LIB -DCOMPONENT_MW_CORE_MAKE -DCOMPONENT_MW_FREERTOS -DCOMPONENT_MW_MTB_HAL_CAT1 -DCOMPONENT_MW_MTB_LITTLEFS -DCOMPONENT_MW_MTB_PDL_CAT1 -DCOMPONENT_MW_RECIPE_MAKE_CAT1C -DCOMPONENT_MW_RETARGET_IO -DCOMPONENT_RTOS_AWARE -DCOMPONENT_SOFTFP -DCOMPONENT_XMC7x_CM0P_SLEEP -DCORE_NAME_CM7_0=1 -DCY_APPNAME_mtb_example_psoc6_filesystem_littlefs_freertos -DCY_RETARGET_IO_CONVERT_LF_TO_CRLF -DCY_SUPPORTS_DEVICE_VALIDATION -DCY_TARGET_BOARD=APP_KIT_XMC71_EVK_LITE_V1 -DCY_USING_HAL -DDEBUG -DLFS_THREADSAFE -DTARGET_APP_KIT_XMC71_EVK_LITE_V1 -DXMC7100D_F176K4160 -I. -Ibsps/TARGET_APP_KIT_XMC71_EVK_LITE_V1 -Ibsps -Ibsps/TARGET_APP_KIT_XMC71_EVK_LITE_V1/config/GeneratedSource -Ibsps/TARGET_APP_KIT_XMC71_EVK_LITE_V1/config -Ilibs/abstraction-rtos/include -Ilibs/abstraction-rtos -Ilibs/abstraction-rtos/include/COMPONENT_FREERTOS -Ilibs/cat1cm0p/COMPONENT_CAT1C -Ilibs/cat1cm0p -Ilibs/clib-support -Ilibs/clib-support/TOOLCHAIN_GCC_ARM -Ilibs/cmsis/Core/Include -Ilibs/cmsis/Core -Ilibs/cmsis -Ilibs/core-lib/include -Ilibs/core-lib -Ilibs/freertos/Source/include -Ilibs/freertos/Source -Ilibs/freertos -Ilibs/freertos/Source/portable/COMPONENT_CM7 -Ilibs/freertos/Source/portable -Ilibs/freertos/Source/portable/COMPONENT_CM7/TOOLCHAIN_GCC_ARM -Ilibs/mtb-hal-cat1/COMPONENT_CAT1C/include/pin_packages -Ilibs/mtb-hal-cat1/COMPONENT_CAT1C/include -Ilibs/mtb-hal-cat1/COMPONENT_CAT1C -Ilibs/mtb-hal-cat1 -Ilibs/mtb-hal-cat1/COMPONENT_CAT1C/include/triggers -Ilibs/mtb-hal-cat1/include -Ilibs/mtb-hal-cat1/include_pvt -Ilibs/mtb-hal-cat1/source -Ilibs/mtb-pdl-cat1/devices/COMPONENT_CAT1C/include -Ilibs/mtb-pdl-cat1/devices/COMPONENT_CAT1C -Ilibs/mtb-pdl-cat1/devices -Ilibs/mtb-pdl-cat1 -Ilibs/mtb-pdl-cat1/devices/COMPONENT_CAT1C/include/ip -Ilibs/mtb-pdl-cat1/drivers/include -Ilibs/mtb-pdl-cat1/drivers -Ilibs/mtb-pdl-cat1/drivers/third_party/ethernet/include -Ilibs/mtb-pdl-cat1/drivers/third_party/ethernet -Ilibs/mtb-pdl-cat1/drivers/third_party -Ilibs/retarget-io -I../mtb_shared/mtb-littlefs/latest-v2.X/bd -I../mtb_shared/mtb-littlefs/latest-v2.X -I../mtb_shared/mtb-littlefs/latest-v2.X/include
../mtb_shared/mtb-littlefs/latest-v2.X/source/lfs_qspi_memslot.c:487:5: error: 'cy_stc_smif_mem_device_cfg_t' has no member named 'mergeTimeout'
487 | .mergeTimeout = CY_SMIF_MERGE_TIMEOUT_1_CYCLE
| ^
make[1]: *** [libs/core-make/make/core/build.mk:283: C:/Users/Prasad/mtw/Littlefs_Filesystem/Littlefs_Filesystem/build/APP_KIT_XMC71_EVK_LITE_V1/Debug/ext/mtb_shared/mtb-littlefs/latest-v2.X/source/lfs_qspi_memslot.o] Error 1
make: *** [libs/core-make/make/core/main.mk:385: secondstage_build] Error 2
"C:/Users/Prasad/ModusToolbox/tools_3.2/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_IDE_TOOLS_DIR=C:/Users/Prasad/ModusToolbox/tools_3.2 CY_IDE_BT_TOOLS_DIR= -j8 --output-sync all" terminated with exit code 2. Build might be incomplete.
When I comment the line:
#if (CY_IP_MXSMIF_VERSION >= 2)
/** Continuous transfer merge timeout.
* After this period the memory device is deselected. A later transfer, even from a
* continuous address, starts with the overhead phases (command, address, mode, dummy cycles).
* This configuration parameter is available for CAT1B devices. */
//.mergeTimeout = CY_SMIF_MERGE_TIMEOUT_1_CYCLE
#endif /* CY_IP_MXSMIF_VERSION */
I get failed to creat spi device block:
Could someone help me with ".mergeTimeout = CY_SMIF_MERGE_TIMEOUT_1_CYCLE" error?
When using the mtb-littlefs through the mtb-shared, how do I enable the cy_hal, freertos and thread in make file?
I tried to add the necessary comments on my application makefile but it is not enabling the corresponding if condition in the files in mtb-shared folder/mtb-littlefs!
best regard,
PrasadA
Show Less
I can program the psoc5 using openocd now, with some caveats. However, if an NVL entry exists, it stops.
I have a project which somehow did something to the NVL.
I understand setting the Reset condition on the Pins can cause this. However, setting the pins to Don't Care doesn't fix this problem, so I suspect something else is causing the NVL to change.
Is there *any* gui / command line interface to find out what is causing the NVL to be set? (so it can be "fixed" in the project?)
This would not normally be a problem, but using openocd to program the psoc halts when the NVL entry is in the Creator generated hex file. I have multiple reasons for using openocd, some of which involve production machines. Others are very fast compile/debug cycle. (https://socmaker.com/?p=1004, and https://socmaker.com/?p=1027)
If I use objcopy, could I exclude that from the elf file for the new obj? (before making a hex file) If so, would it be by address? If so, which address? otherwise, how would I do that exclusion?
Is there a way to use openocd to program the NVL (perhaps kitprog in kitprog mode?) (Just checking)
Thanks!
Show Less
Hello!
I have the following code that is not working. After first call of readRegister response is 0, after calling readRegister the second time, I receive the expected value.
Can you please help? I must mention that my application is based on the Infineon SPI_CPU_TC334 training and I've also tried to change spiMasterChannelConfig.channelBasedCs but I still don't receive the expected behavior.
I've also attached the source code for QSPI.
Thank you!
/**********************************************************************************************************************
* \file Cpu0_Main.c
* \copyright Copyright (C) Infineon Technologies AG 2019
*
* Use of this file is subject to the terms of use agreed between (i) you or the company in which ordinary course of
* business you are acting and (ii) Infineon Technologies AG or its licensees. If and as long as no such terms of use
* are agreed, use of this file is subject to following:
*
* Boost Software License - Version 1.0 - August 17th, 2003
*
* Permission is hereby granted, free of charge, to any person or organization obtaining a copy of the software and
* accompanying documentation covered by this license (the "Software") to use, reproduce, display, distribute, execute,
* and transmit the Software, and to prepare derivative works of the Software, and to permit third-parties to whom the
* Software is furnished to do so, all subject to the following:
*
* The copyright notices in the Software and this entire statement, including the above license grant, this restriction
* and the following disclaimer, must be included in all copies of the Software, in whole or in part, and all
* derivative works of the Software, unless such copies or derivative works are solely in the form of
* machine-executable object code generated by a source language processor.
*
* THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE
* WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT. IN NO EVENT SHALL THE
* COPYRIGHT HOLDERS OR ANYONE DISTRIBUTING THE SOFTWARE BE LIABLE FOR ANY DAMAGES OR OTHER LIABILITY, WHETHER IN
* CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS
* IN THE SOFTWARE.
*********************************************************************************************************************/
#include "Ifx_Types.h"
#include "IfxCpu.h"
#include "IfxScuWdt.h"
#include "QSPI_Config.h"
#include "Timers.h"
#define LED &MODULE_P00,5
IFX_ALIGN(4) IfxCpu_syncEvent g_cpuSyncEvent = 0;
volatile uint8 delay;
static unsigned char response = 0;
void core0_main(void)
{
IfxCpu_enableInterrupts();
/* !!WATCHDOG0 AND SAFETY WATCHDOG ARE DISABLED HERE!!
* Enable the watchdogs and service them periodically if it is required
*/
IfxScuWdt_disableCpuWatchdog(IfxScuWdt_getCpuWatchdogPassword());
IfxScuWdt_disableSafetyWatchdog(IfxScuWdt_getSafetyWatchdogPassword());
/* Wait for CPU sync event */
IfxCpu_emitEvent(&g_cpuSyncEvent);
IfxCpu_waitEvent(&g_cpuSyncEvent, 1);
//init1msTimer();
initQSPI2Master();
initQSPI2MasterChannel();
resetIMMU();
selfTestIMMU();
/*uint8 xGyro, yGyro, zGyro;*/
while(1)
{
response = readRegister(WHO_AM_I, 0x00);
// response = readRegister(WHO_AM_I, 0x00);
//readIMMUAxis(&xGyro, &yGyro, &zGyro);
}
}
Show Less
您好,我在使用xmc4800,ethercat。这个示例代码ETHCAT_SSC_AUT_BASE_XMC48里添加PMSM_FOC组件,报了两个错误,我在单独使用PMSM_FOC这个工程正常编译运行。但在ETHCAT_SSC_AUT_BASE_XMC48就会出现这两个问题,请看附件图
多次尝试无法解决,请帮看一下。感谢!!!
Show LessDear All,
I use the DAVE ide v4 with the nano library, calling the SPI-MASTER-EnableSlaveSelectSignal() and SPI-MASTER-DisableSlaveSelectSignal() functions cannot raise or lower the CS pin of SPI. However, when sending data through SPI, when using an oscilloscope to check the status of SCL and MOSI pins, they generate waveforms that are normal, but the CS pin remains in a high level state.
Configure this CS pin as an IO port, manually pull up or down the CS pin, but use the BUSY flag in the TBUF register as the completion of sending. When pulling up the CS pin, there will be a situation where there is still one byte that has not been sent, but the CS pin has been pulled up.
What may be the reason why the two API functions generated by calling cannot control the CS pin state; How can I avoid manually raising or lowering the CS pin when there is still one byte of data not sent?
Thanks.
Show LessHi
I want to know sleep current of TLE9853QX & also it auto wake when LIN signal is available. My customer is using in Flush door handle.
I have seen multiple sleep mode specs available in datasheet but not able to understand actual avg sleep mode current required.
Regards
Lucky Kumar
Show Less
TL9183Q MLCC Chip Capacitor for Charge Pump CB 4.7uF It is prone to whistling, and replacing it with a larger or smaller capacitor value does not improve it much.
Any good solutions?
Show LessHi,
I am having the Traveo-T2G kit. CYTVII-2D-4M-216 set and the CYT3DLABHBES cpu.
I am running the TRAVEO T2G Sample driver Library provided by infineon. I want to use freeRTOS in the project.
Previously I was using IAR V9.30.1 , in that version I could see the option in workspace to switch to the RTOS supported workspace.
Now I am using IAR v8.22.2, here no option in workpace for RTOS. Can somebody help me to run RTOS example.
Show Less
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023