Legacy microcontrollers Forum Discussions
Hi, I'm new to the Infineon microcontroller family, presently there is a requirement to do the development with the Xc836 microcontroller.
can you please suggest, how to start with, which IDE I have to use, and what tools are required for the programming?
Show LessWe can use excel file to input motor parameter and compile the FOC motor driving project.
We got .hex file for downloading to MCU XC878.
Our application board can start motor as open loop.
Then motor has a little vibration and fail for running. (I think it cannot get in close loop control)
My question:
We need to adjust some parameter on excel file right?
We don't have experience for tuning XC878 motor drive.
If you have experience, could you guide us step-by-step ?
Thank you.
Best Regards,
iamten Show Less
I'm new to the Infineon. I'm using XC836 8-bit microcontroller, can anyone suggest the, which IDE and debuggers I have to use for above mentioned microcontroller
Show LessHi,
I was writing data to the main Flash using 16bit, and there was a discrepancy between the data read and the data written. I used the reference routine to simplify the code that could cause problems.
Best regards,
Thanks
Show LessHi Dear,
We used to use CY96F348HSCPQC-GSE2 and CY96F348HSBPQCR-GSE2 for our controller, now we need produce some controllers for our customer, and they are both obsolete part now, when I check discontinued product function for them, Infineon official website shows both of these 2 parts don't have replacement, could you please advise some solution or suggest any simillar part(s) for thess 2 parts,
Many thanks with kind regards.
Steven Song
Show LessHi. I need a tool for read and write this MCU. INFINEON sak-c505ca-4em
Please let me know the details.
I'm trying to figure out how to erase PFlash1 sector 0.
Give me a hint please should I use the following settings?
ST = 0xA0000000;
SA = 0xA0800000; // PFlash1 S0?
Erase Sector
Calling:
• ST 5554 H , xxAA H
• ST AAA8 H , xx55 H
• ST 5554 H , xx80 H
• ST 5554 H , xxAA H
• ST AAA8 H , xx55 H
• ST SA, xx30 H
Function:
The sector “SA” is erased.
Show Less
could you please answer the following question we received via social media?
Question: Why DC to DC? What's the use case?
Here is the link to our post: https://www.facebook.com/345383962211058/posts/5777023409047059/
Show LessHello at all,
I have an Infineon XE167 microcontroller in an older project. Now I have to search an issue. But we have no Debugger in the company for Infineon microcontrollers.
Which debugger do i need to debug on this controller.
Thanks in advance.
Show Less