Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
Hello,

XMC-Link-Segger:
http://www.infineon.com/cms/en/product/evaluation-boards/KIT_XMC_LINK_SEGGER_V1/productType.html?pro...


  • What is the maximum JTAG/SWD speed?
  • Are unlimited breakpoints enabled?
  • Is J-Flash enabled?
  • Can it be used on other controllers or is it limited to Infineon or even XMC?
0 Likes
3 Replies
Not applicable
Are unlimited breakpoints enabled? why
0 Likes
User7887
Level 1
Level 1
Hi Holger

1. The speed up to 4MHz for SWD
2. Yes. but not built-in, need an extra license
3. Yes, as well need an extra license, but you can use Jflash lite without license
4. It should support other Cortex-M microcontroller.

Best wishes

Hongjie
0 Likes