cancel
Showing results for 
Search instead for 
Did you mean: 

Legacy Microcontrollers

vishal854
New Contributor

Hi,

I want to develop an SW for XE167F-96F device, but as I can c it uses the Keil c166 compiler. Can I also use GCC compiler to build the SW or can I port the SW so that it can be built using GCC compiler?

 

Thanks,

Vishal

0 Likes
1 Reply
zzz_3221081
New Contributor II

My company uses an ECU based on a XE22xx controller, which is basically an extension of the C166.

We use Tasking VX, albeit I am not sure if that would be an improvement to Keil's toolchain, both in regard to costs and code quality.

Not sure about free gcc compilers. An equally important point is a toolchain that supports your debug pod, both for programming and debugging. The XE22xx debug interface is not JTAG, I suppose XC166 is the same.

0 Likes