LITIX™ Automotive LED Driver IC

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
fausto_borg
LITIX™ Automotive LED Driver IC
TLD5099EP  can be used with 3.3 V and 5 V microcontrollers without any problems. The EN/PWMI pin thresholds are designed to be compliant with both uC ... Show More
vasiliki
LITIX™ Automotive LED Driver IC
OUT_SET pin mirrors the IIN_SET current set by the external resistor RSET. Any change on the IIN_SET current will be mirrored to the OUT_SET pin.PWM m... Show More
fausto_borg
LITIX™ Automotive LED Driver IC
SEPIC DC-DC converter needs two inductors to properly work. The two inductors can be wrapped on the same core (coupled inductors) or on two separated ... Show More
fausto_borg
LITIX™ Automotive LED Driver IC
With LITIX Power boost controllers it is possible to implement a delay and fade-in / fade-out functions without using a microcontroller.This can be do... Show More
vasiliki
LITIX™ Automotive LED Driver IC
ERRN status remains low when the fault is present on the output even during the IN_SET de-activation time (IN_SET open via uC).This happens because ER... Show More
vasiliki
LITIX™ Automotive LED Driver IC
GNDS-pin must be connected to GND and can't be left open.For more information check the LITIX™ Basic webpage. Show More
User22521
LITIX™ Automotive LED Driver IC
Hi everyoneI am looking at playing around with the TLD5099. I realise its aimed at LED drivers but I would like to make small DC-DC power supplies. A ... Show More
vasiliki
LITIX™ Automotive LED Driver IC
The pull-up resistor at ST-pin is calculated according to following equation:RST > VREG/IST, where VREG is the pull-up voltage for the ST-pin (see IST... Show More
vasiliki
LITIX™ Automotive LED Driver IC
The minimum current of LITIX™ Basic+ is limited by the IN_SET output activation current, IIN_SET(ACT) (data sheet parameter P_6.2.2): IOUTmin = IIN_SE... Show More
fausto_borg
LITIX™ Automotive LED Driver IC
The TLD509x mainly differ in maximum output voltage, output current accuracy, analog dimming, short-to-ground protection and capability to drive an ex... Show More
Top liked authors