Sep 28, 2021
12:31 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 28, 2021
12:31 AM
With LITIX Power boost controllers it is possible to implement a delay and fade-in / fade-out functions without using a microcontroller.
This can be done by using filters with different time constant at the SET pin. The SET pin is the analog adjustment input and it is used to control the output current. One of the filters needs to be switchable.
In the example below
Filter 1 is a low pass filter that enables and disables the output current with a defined delay by closing or opening the MOSFET
Filter 2 is a low pass filter that enables the fade-in/fade-out function.
For further details you can also visit LITIX Power webpage
This can be done by using filters with different time constant at the SET pin. The SET pin is the analog adjustment input and it is used to control the output current. One of the filters needs to be switchable.
In the example below
Filter 1 is a low pass filter that enables and disables the output current with a defined delay by closing or opening the MOSFET
Filter 2 is a low pass filter that enables the fade-in/fade-out function.
For further details you can also visit LITIX Power webpage
- Tags:
- IFX
- litix power
0 Replies