LED Driver ICs Forum Discussions
Does .dp vision, the software for using .dp Interface Gen2, support windows 11?
I have even confirmed that it works on windows 10.
However, I am receiving inquiries from customers that it does not work on windows 11 .
Hi,
We design a board with the TLD7002-16ES led driver.
How can I get samples for testing?
I am interfacing SPI module of SPC560DL40L3 microcntroller with TLE75008 to drive 5 relays.may i get some source or sample code for same.
What's the RPOL and DPOL function for TLD5099EP?
Dear Team
we are using the device IR2156, SOIC 16 package for developing a SMPS supply , of 500W.
We are facing difficult time in sourcing the device.
can u please suggest the another device equivalent or better than IR2156
LOOKING FOR THE PROMPT REPLY.
rgds
yogesh singhal
Show Less
Greetings,
When attempting to debug an XDPL8210 LED driver using .dp Vision, I follow the instructions in the XDPL2010 Design Guide 2022-08-09 page 48.
An error dialog pops up with "APP_WARM_START" or "NAK_UART_DISABLED". What causes this?
Many Thanks
Show LessWe need to design the AR-HUD backlight application.
Could you provide the minimum output dimming duty in digital PWM?
Minimum Frequency range?
Hi,
I'm looking to power and control the dimming for an AMOLED display, and was looking for help in how to connect the power and dimming of the amoled. To my understanding, AMOLED displays don't have a backlight, so it's not possible to change the brightness of the actual display. Instead, you can change the voltage/current or the duty cycle of the power to the display to change the brightness.
I'm planning on using an STM32 processor and getting power from USB-C connected to a computer or laptop. I believe that I need a display bias PMIC as a power supply for the display, but I'm not sure how/what dimming solution fits into the circuit.
There's two different types of dimming for OLED: DC dimming and PWM, and I would prefer to use DC dimming, but if it's not possible PWM is fine as well.
For PWM, do I simply connect the output of the display bias to a transistor and change the duty cycle to change the brightness of the display?
If there was any recommendations for chips to use and their circuit configurations that would be greatly appreciated.
Thanks!
Show LessHello,
I'm writing code for communicating with a TLD7002 for a development tool, and would like to ask a few questions concerning the calculation of the CRC sums. As the driver library is not yet available to me, I'm implementing basic access to the HSLI in the programming language I'm using.
The datasheet of the TLD7002-16ES specifies two types of CRC algorithms, a 3-bit CRC, and an 8-bit CRC.
1. Regarding the 3-bit CRC, in the software design training video there appears a step where the crc value is reflected (mirrored) after processing the first 5 bits:
/* get reflected CRC3 value */
crc = TLD7002_MIRROR_MID_CRC3[crc];
I cannot find this step in the datasheet on page 67, though — an extra step reflecting the crc value after the first 5 bits and the tail 8 bits is not mentioned there; is the datasheet correct regarding the calculation of the 3-bit CRC?
2. The CRC-8 is defined as using the generator polynomial "0x8e = x^8 +x^4 +x^3 +x^2 +1" from CRC-8-AUTOSAR and SAE J1850.
But, from my understanding, 0x8E — binary: (1)-1000-1110 — actually is not the same as x⁸ + x⁴ + x³ + x² + 1;
0x8E is the reversed — LSB-first — form of 0x71 (1)-0111-0001, which corresponds to the polynomial x⁸ + x⁶ + x⁵ + x⁴ + 1, and is the reciprocal form, or Koopman representation, of the CRC-8-SAE polynomial 0x1D, but with similar properties:
(Source: Wikipedia)
So if the polynomial actually is 0x8E, then for calculating the CRC-8 of the safety byte the reversed, LSB first, algorithm would have to be used. Is this correct?
If yes, then this possibly also applies to the CRC-3, because two CRC sums used in the same HSLI frame are likely implemented in the same fashion. This could mean that the polynomial to be used when calculating the CRC-3 would be 0x6 ("reversed"), or 0x5 ("reversed reciprocal"), but not 0x3. Which one is actually used by the TLD7002-16ES?
The CRC-8 of SAEJ1850, by the way, also defines a final XOR step, where 0xFF is XOR'ed into the crc value. I suppose, since the datasheet of the TLD7002-16ES does not mention this, this final step of the original SAEJ1850 definition does not need to be performed in case of HSLI?
It could probably be helpful, if a table of example CRC results for various input values would be included in the datasheet, similarly as it is done in the Autosar document Specification of CRC Routines; this way users could perform a test for plausibility of their crc implementations, before sending actual requests to the TLD7002.
Regards,
Michael