Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

LED Driver ICs Forum Discussions

Jsauce9412
Level 1
Level 1
5 sign-ins First question asked Welcome!

We are sending inquiries regarding TLD6098-1EP IC PWM DUTY 

We are trying to apply in Daytime Running Lamp, Position Lamp.

 

1) Is it possible to control the  PWM duty cycle 5% in the IC to satisfy the LED minimum guaranteed current?

2) Due to low dimming control such as Analog Dimming (SET) PIN 30% control and PWM DUTY 5% control
Can output current error and flicker occur?

0 Likes
1 Solution
AliAsgar
Moderator
Moderator
Moderator
250 solutions authored 750 replies posted 50 likes received

Hi,

Regarding the flickering, I assume you are talking about instability that could trigger the light flickering. Usually if the PWM frequency is higher than 50Hz then it is not visible.

  • 5% is achievable if a PMOS is used as dimming element.
  • The flickering depends on stability. If a proper compensation network is chosen, then there shouldnt be a problem.

Please check the TLD6098-12B_EVAL evaluation kit and check the stability with DC-DC designer tool

Best Regards,
AliAsgar

View solution in original post

1 Reply
AliAsgar
Moderator
Moderator
Moderator
250 solutions authored 750 replies posted 50 likes received

Hi,

Regarding the flickering, I assume you are talking about instability that could trigger the light flickering. Usually if the PWM frequency is higher than 50Hz then it is not visible.

  • 5% is achievable if a PMOS is used as dimming element.
  • The flickering depends on stability. If a proper compensation network is chosen, then there shouldnt be a problem.

Please check the TLD6098-12B_EVAL evaluation kit and check the stability with DC-DC designer tool

Best Regards,
AliAsgar

This widget could not be displayed.