Announcements

Register now for the most anticipated Asia Pacific Power Seminar 2022

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

LED Driver ICs Forum Discussions

fausto_borg
Moderator
Moderator 10 likes received 10 sign-ins 5 solutions authored
Moderator
With LITIX Power boost controllers it is possible to implement a delay and fade-in / fade-out functions without using a microcontroller.

This can be done by using filters with different time constant at the SET pin. The SET pin is the analog adjustment input and it is used to control the output current. One of the filters needs to be switchable.

In the example below

Filter 1 is a low pass filter that enables and disables the output current with a defined delay by closing or opening the MOSFET
Filter 2 is a low pass filter that enables the fade-in/fade-out function.

5421.attach

For further details you can also visit LITIX Power webpage
0 Replies