Announcements

Register now for the most anticipated Asia Pacific Power Seminar 2022

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

LED Driver ICs Forum Discussions

User20729
Level 1
5 questions asked First question asked
Level 1
Does the TLD1211 support such protection functions?
0 Likes
1 Solution
vasiliki
Employee
25 sign-ins 5 questions asked First question asked
Employee
Hello,

The TLD1211SJ reacts on OL or SC according to the following table:
4955.attach

Please note that as the control loop in open load and short circuit behaves the same (VSENSE ~0V), the current consumption is expected to be the same for the two faults, <1.7 mA (parasitic effects could make some difference).

The TLD1211SJ is also protected against overload, overvoltage and overtemperature. In case of those faults the output current will decrease, protecting not only the IC but also the LEDs.
Please refer to the datasheet of TLD1211SJ for more details.

View solution in original post

1 Reply
vasiliki
Employee
25 sign-ins 5 questions asked First question asked
Employee
Hello,

The TLD1211SJ reacts on OL or SC according to the following table:
4955.attach

Please note that as the control loop in open load and short circuit behaves the same (VSENSE ~0V), the current consumption is expected to be the same for the two faults, <1.7 mA (parasitic effects could make some difference).

The TLD1211SJ is also protected against overload, overvoltage and overtemperature. In case of those faults the output current will decrease, protecting not only the IC but also the LEDs.
Please refer to the datasheet of TLD1211SJ for more details.