Moderator

Moderator
Jul 05, 2021
12:10 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Our LITIX boost controllers like TLD5099EP have two options to dim the output current without a microcontroller:
- Analog current adjustment
- Embedded PWM engine
In the system these two options can be used to:
- Adjust the output current as a function of binning resistor
- Thermal foldback (thermal protection)
The two functions are activated by analog voltages at the pins SET and PWMI - e.g. by resistor dividers. Then are no interferences between these two functions.
See the datasheets at our LITIX pages
- Analog current adjustment
- Embedded PWM engine
In the system these two options can be used to:
- Adjust the output current as a function of binning resistor
- Thermal foldback (thermal protection)
The two functions are activated by analog voltages at the pins SET and PWMI - e.g. by resistor dividers. Then are no interferences between these two functions.
See the datasheets at our LITIX pages
0 Replies