Moderator

Moderator
Nov 19, 2020
07:04 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
In total you can use up to 11 LITIX™ BASIC+ LED driver devices for one function on the same ERRN bus.
Rationale:
Referring to the ECs (Electrical Characteristics) "internal supply and EN pin" two parameters are of interest:
So in total you can use 11 devices in one function since 1.25mA+(11-1)*0.85mA=9.75mA<10mA.
Find the datasheets and application notes at the LITIX Basic+ page.
Rationale:
Referring to the ECs (Electrical Characteristics) "internal supply and EN pin" two parameters are of interest:
- IS(fault,ERRN): Current consumption during fault condition triggered from another device sharing ERRN bus (all channels deactivated) is < 0.85 mA
- IS(fault,OUT) Current consumption during fault condition (all channels deactivated) is < 1.25mA
So in total you can use 11 devices in one function since 1.25mA+(11-1)*0.85mA=9.75mA<10mA.
Find the datasheets and application notes at the LITIX Basic+ page.
- Tags:
- IFX
0 Replies