Level 1
User20590
Level 1
Jan 19, 2021
09:05 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Can your H-bridge drivers be operated with less than four MOSFETs in pure buck mode?
Solved! Go to Solution.
- Tags:
- IFX
1 Solution
Moderator

Moderator
Jan 20, 2021
12:19 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
In order to save BOM cost it is possible to use our H-Bridge drivers with 2 MOSFETs only.
TLD5190QV, TLD5190QU, TLD5542-1QV and TLD5542-1QU will turn on the low side gate drivers in error conditions. Then the following fault behaviors have to be considered:
* Short-to-battery: battery is getting discharged via the low side MOSFET M2 without current limitation (destructive for the discharge path)
* Overvoltage or open load: Output capacitor is getting discharged via lows side MOSFET M2 without current limitation
In order to avoid such discharge currents without current limitation the highside MOSFET M4 of the H-bridge may also be replaced by a power diode instead of a short-circuit.
When using the diode please consider the voltage drop for the duty cycle calculation (D = (Vout+Vdiode)/Vin).
Please also connect BST2 to IVCC and SWN2 to GND in order to avoid triggering undervoltage on BST2.
During input transients the device could go in buck-boost or boost mode and behave similar to normal buck controllers stopping to regulate at the maximum duty cycle.
E.g. see the product pages of TLD5190QV and TLD5542-1QV
TLD5190QV, TLD5190QU, TLD5542-1QV and TLD5542-1QU will turn on the low side gate drivers in error conditions. Then the following fault behaviors have to be considered:
* Short-to-battery: battery is getting discharged via the low side MOSFET M2 without current limitation (destructive for the discharge path)
* Overvoltage or open load: Output capacitor is getting discharged via lows side MOSFET M2 without current limitation
In order to avoid such discharge currents without current limitation the highside MOSFET M4 of the H-bridge may also be replaced by a power diode instead of a short-circuit.
When using the diode please consider the voltage drop for the duty cycle calculation (D = (Vout+Vdiode)/Vin).
Please also connect BST2 to IVCC and SWN2 to GND in order to avoid triggering undervoltage on BST2.
During input transients the device could go in buck-boost or boost mode and behave similar to normal buck controllers stopping to regulate at the maximum duty cycle.
E.g. see the product pages of TLD5190QV and TLD5542-1QV
1 Reply
Moderator

Moderator
Jan 20, 2021
12:19 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
In order to save BOM cost it is possible to use our H-Bridge drivers with 2 MOSFETs only.
TLD5190QV, TLD5190QU, TLD5542-1QV and TLD5542-1QU will turn on the low side gate drivers in error conditions. Then the following fault behaviors have to be considered:
* Short-to-battery: battery is getting discharged via the low side MOSFET M2 without current limitation (destructive for the discharge path)
* Overvoltage or open load: Output capacitor is getting discharged via lows side MOSFET M2 without current limitation
In order to avoid such discharge currents without current limitation the highside MOSFET M4 of the H-bridge may also be replaced by a power diode instead of a short-circuit.
When using the diode please consider the voltage drop for the duty cycle calculation (D = (Vout+Vdiode)/Vin).
Please also connect BST2 to IVCC and SWN2 to GND in order to avoid triggering undervoltage on BST2.
During input transients the device could go in buck-boost or boost mode and behave similar to normal buck controllers stopping to regulate at the maximum duty cycle.
E.g. see the product pages of TLD5190QV and TLD5542-1QV
TLD5190QV, TLD5190QU, TLD5542-1QV and TLD5542-1QU will turn on the low side gate drivers in error conditions. Then the following fault behaviors have to be considered:
* Short-to-battery: battery is getting discharged via the low side MOSFET M2 without current limitation (destructive for the discharge path)
* Overvoltage or open load: Output capacitor is getting discharged via lows side MOSFET M2 without current limitation
In order to avoid such discharge currents without current limitation the highside MOSFET M4 of the H-bridge may also be replaced by a power diode instead of a short-circuit.
When using the diode please consider the voltage drop for the duty cycle calculation (D = (Vout+Vdiode)/Vin).
Please also connect BST2 to IVCC and SWN2 to GND in order to avoid triggering undervoltage on BST2.
During input transients the device could go in buck-boost or boost mode and behave similar to normal buck controllers stopping to regulate at the maximum duty cycle.
E.g. see the product pages of TLD5190QV and TLD5542-1QV