Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Mac_Komatsubara
Level 3
Level 3
Distributor - Macnica (Japan)
5 replies posted First solution authored 25 sign-ins

There are two thresholds for the EN/DEN pin: output enable and diagnosis enable.
If the terminal voltage is 2V, the output enable (threshold 1.8V or less) reaches the threshold, but the diagnosis enable (threshold 2.4V or more) does not reach the threshold.
I think diagnosis does not work under those conditions, but current still be output from the OUT pin?

0 Likes
1 Solution
Kanahaiya_K
Moderator
Moderator
Moderator
50 likes received 100 solutions authored 10 likes given

Hi @Mac_Komatsubara ,
Thanks for posting on the Infineon Developer Community.

The EN output enable threshold VEN(th) & DEN diagnosis enable threshold VDEN(th) are 1.65 volt & 2.5 volt respectively. The typical value of VDEN(th) signifies that 2.5 Volts of input voltage is required at the DEN pin to activate the diagnosis whereas the typical value of VEN(th) signifies that 1.65 Volts of input voltage is required at the EN pin to enable the output.

Yes,your observation is correct.The output will be activated and you can obtain the output as soon as the voltage at the input pin reaches the VEN threshold but the diagnosis of the device will not work if the VDEN thresthold is not reached.

I hope the information will be useful for you.

Please feel free to contact in case of any further clarifications.

Best Regards,
Kanahaiya

View solution in original post

1 Reply
Kanahaiya_K
Moderator
Moderator
Moderator
50 likes received 100 solutions authored 10 likes given

Hi @Mac_Komatsubara ,
Thanks for posting on the Infineon Developer Community.

The EN output enable threshold VEN(th) & DEN diagnosis enable threshold VDEN(th) are 1.65 volt & 2.5 volt respectively. The typical value of VDEN(th) signifies that 2.5 Volts of input voltage is required at the DEN pin to activate the diagnosis whereas the typical value of VEN(th) signifies that 1.65 Volts of input voltage is required at the EN pin to enable the output.

Yes,your observation is correct.The output will be activated and you can obtain the output as soon as the voltage at the input pin reaches the VEN threshold but the diagnosis of the device will not work if the VDEN thresthold is not reached.

I hope the information will be useful for you.

Please feel free to contact in case of any further clarifications.

Best Regards,
Kanahaiya