Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Knowledge Base Articles

Knowledge Base Articles

Recent documents

Sort by:
BinduPriya_G
Knowledge Base Articles
Version: **In addition to DMA descriptors for Single, 1D and 2D transfers the Peripheral DMA (P-DMA) in TRAVEO™ T2G also supports a Cyclic Redundancy... Show More
BinduPriya_G
Knowledge Base Articles
Version: **GTM (Generic Timer Module) implemented in AURIX™ TC2xx supports only up counter mode. GTM implemented in AURIX™ TC3xx supports up-down cou... Show More
BinduPriya_G
Knowledge Base Articles
Version: **In the VADC module, one ADC converter has one dedicated Sample&Hold unit (no multiple S&H units). Therefore, the maximum number of analog ... Show More
BinduPriya_G
Knowledge Base Articles
Version: ** There is no specific crystal recommendation for AURIX™ MCUs. All typical crystals in the market in the specified frequency range should r... Show More
BinduPriya_G
Knowledge Base Articles
Version: ** If the Auto-discover compiler include paths is disabled, right-click on the folder to quickly add or remove a folder from the compiler inc... Show More
BinduPriya_G
Knowledge Base Articles
Version: **To create a library project in AURIX™ Development Studio, do the following: Click File > New > New AURIX™ Project from the AURIX™ Develo... Show More
BinduPriya_G
Knowledge Base Articles
Version: **The metadata of an object can be changed if the Life cycle state Object (LcsO) of the object is not in operational or termination state. I... Show More
MohammedA_41
Knowledge Base Articles
Version: ** In AURIX™ MCUs, program flash has 20 years of data retention time while the data flash has 10 years. Because the program flash is written... Show More
BinduPriya_G
Knowledge Base Articles
Version: **The tools available in the toolchain, enables the user to manually add flags by editing the Command line pattern under the Expert settings... Show More
BinduPriya_G
Knowledge Base Articles
Version: **In AURIX™ TC2xx, the maximum GTM (Generic Timer Module) clock frequency is 100 MHz; therefore, the highest resolution can be 10 ns. In AURI... Show More
BinduPriya_G
Knowledge Base Articles
Version: **The exposed die pad is used for cooling purposes and to allow better heat dissipation. It should be placed on the bottom side of the VQFN-... Show More
BinduPriya_G
Knowledge Base Articles
Version: **The net bandwidth, which can be achieved with HSSL, varies in a wide range from just a fraction up to ~82% of the maximal available bandwi... Show More
BinduPriya_G
Knowledge Base Articles
Version: **This KBA presents the results of performance measurements performed on different combinations of locations of source and store buffers usi... Show More
Neo_Lu
Knowledge Base Articles
In the magnetic sensor development tool, Infineon provides complete supporting software and source code based on Arduino platform; However, this arti... Show More
BinduPriya_G
Knowledge Base Articles
Version: **The primary monitor operation is based on tracking an analog-to-digital converter (ADC) to measure the supply voltages. It is clocked and ... Show More
BinduPriya_G
Knowledge Base Articles
Version: **On the AURIX™ TC2XX devices, the modulator and demodulator are used together; therefore, delta-sigma analog-to-digital converter (DSADC) d... Show More
BinduPriya_G
Knowledge Base Articles
Version: **The default switching frequency is 1.5 MHz during embedded voltage regulator (EVR) start up and you can configure this frequency between 0... Show More
BinduPriya_G
Knowledge Base Articles
Version: **For a parallel conversion, up to four Analog-to-Digital Converter (ADC) in a synchronization group can be exactly synchronized. In case of... Show More
BinduPriya_G
Knowledge Base Articles
Version: **There are two types of NC balls: NC: Not Connected. These pins are reserved for future extensions and shall not be connected externally. ... Show More
BinduPriya_G
Knowledge Base Articles
Version: **Input voltage high for S pad (VIHS) and input voltage low (VILS) for S pad are as follows: For AURIX™ TC2xx MCU series: VDDM = 5 V ... Show More
Knowledge Base Information

Knowledge Base Articles

Knowledge Base Articles are product related resources written by our Apps Team Experts.
Top contributors