Knowledge Base Articles

cancel
Showing results for 
Search instead for 
Did you mean: 
Create an article

Knowledge Base Articles

Recent documents

Sort by:
Chelladurai
Knowledge Base Articles
Version: ** You cannot use S29GL256S as primary booting memory for Xilinx Zynq-7000 SoC because S29GL256S supports x16 data width and does not have a... Show More
Chelladurai
Knowledge Base Articles
Version: ** The Verilog/VHDL model for Infineon NOR flash device is available to download here. After downloading the file, see Model Manual in the f... Show More
Chelladurai
Knowledge Base Articles
Version: ** Is the XENSIVTM PAS CO2 sensor affected by acoustic and vibration noise?XENSIVTM PAS CO2 sensor has a robust packaging, and is acoustica... Show More
Chelladurai
Knowledge Base Articles
Version: ** VLKO is the lock-out voltage of the core power supply (VCC). The intention of VLKO is to make sure that device is on expected VCC level b... Show More
Chelladurai
Knowledge Base Articles
Version: ** Wait states and dummy cycles are the same. Read latency is superset of wait states (or dummy cycles). Read latency equals the sum of cloc... Show More
Chelladurai
Knowledge Base Articles
Version: ** Question: Can noise on the power supply rail cause a ‘bit-flip’, and damage on the S29AL-J, S29PL-J, and S29JL-J flash memory devices? An... Show More
Chelladurai
Knowledge Base Articles
Version: ** Consider the following table to calculate the dimensions for SMD and NSMD pad types when designing hardware with BGA package FAB024 for o... Show More
Chelladurai
Knowledge Base Articles
Version: **   Two types of land pad patterns are solder mask defined (SMD) pad and non-solder mask defined (NSMD) pad. The land pad pattern type diff... Show More
ArunKumarChoul
Knowledge Base Articles
Version: **1. RFU (Reserved For Future Use) No device internal signal is currently connected to the package. However, there is potential future use o... Show More
Chelladurai
Knowledge Base Articles
Version: ** S28HL-T and S28HS-T series SEMPER™ NOR flash with Octal interface can support legacy SPI (x1) mode and Octal (x8) mode, with legacy SPI a... Show More