Knowledge Base Articles

cancel
Showing results for 
Search instead for 
Did you mean: 
Create an article

Knowledge Base Articles

Recent documents

Sort by:
Chelladurai
Knowledge Base Articles
Version: ** When the CAPSENSE™ shield is enabled, the shield hatch is driven to the same potential as the sensors during the charging and discharging... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Context:The reset status is always set as ‘software reset’ in a bootloadable project for PSoC™ 3/4/5LP MCUs even though the device is res... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** The PSoC™ programmer command-line interface (PPCLI) tool in the PSoC™ programmer installation directory (C:\Program Files (x86)\Cypress\P... Show More
Chelladurai
Knowledge Base Articles
Version: ** Problem: PSoC™ 3 MCU, PSoC™ 4 MCU, PSoC™ 5LP MCU, and some of PSoC™ 6 MCU devices have a powerful and flexible programmable digital perip... Show More
Chelladurai
Knowledge Base Articles
Version: ** Question: What is the workaround for the connection issue between HTerm  and KitProg3 COM port after the KitProg3 firmware update? Answer... Show More
Chelladurai
Knowledge Base Articles
Version: ** The Motorola SPI protocol has four different modes based on how data is driven and captured on the MOSI and MISO lines. These modes are d... Show More
Chelladurai
Knowledge Base Articles
Version: ** This article is for CMSIS5. For information about a previous CMSIS version, see KBA90457. Do the following to include the CMSIS5 Library ... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Question: How can I specify an alternate tools version for my ModusToolbox application? Answer: You can install multiple ModusToolbox sof... Show More
Chelladurai
Knowledge Base Articles
Version: ** When building a PSoC Creator project that uses UDBs, you may get the error “Unable to pack the design into available UDBs”. This error oc... Show More
Chelladurai
Knowledge Base Articles
Version: ** Both ModusToolbox and Cypress Programmer use OpenOCD underneath to communicate with the device. So, to change the programming clock speed... Show More