Knowledge Base Articles

cancel
Showing results for 
Search instead for 
Did you mean: 
Create an article

Knowledge Base Articles

Recent documents

Sort by:
MohammedA_41
Knowledge Base Articles
Version: ** Implementation In this project, the MUX functionality is implemented with a MUX Component in TopDesign.cysch in PSoC™ Creator while for... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Question: How to create a basic PSoC® Creator project implementing UART functionality, without using UART component in TopDesign.cysch? A... Show More
Chelladurai
Knowledge Base Articles
Version: ** PSoC™ 6 MCU with AIROC™ Bluetooth® LE connectivity supports two types of events: Bluetooth® LE stack events and service-specific events. ... Show More
Chelladurai
Knowledge Base Articles
Version: ** Related products: PSoC™ 6 MCU with AIROC™ Bluetooth® LE You can use the Cy_BLE_GATTS_EnableAttribute() and Cy_BLE_GATTS_DisableAttribute(... Show More
Chelladurai
Knowledge Base Articles
Version: ** In the code, you can read the major version, minor version, patch number, and build number of the Bluetooth® LE stack library by using th... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** PSoC™ 6 MCU devices with USB support have dedicated pins for the D+ and D- USB lines (pins P14[0] and P14[1]). If the USB functionality i... Show More
Chelladurai
Knowledge Base Articles
Version: ** Context The PSoC™ 6 MCU has several Arm®-specified advanced high-performance bus (AHB) interface masters such as Arm® CM4 CPU core, Arm® ... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Affected products: PSoC™ 4 and PSoC™ 6 MCUs with AIROC™ Bluetooth® LE. In Bluetooth® LE GAP Peripheral role, when a device is advertising... Show More
Chelladurai
Knowledge Base Articles
Version: ** Question: What is the workaround for the connection issue between HTerm  and KitProg3 COM port after the KitProg3 firmware update? Answer... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** After reset, the boot code is the first to run, which performs the following sequence of actions: Executes any hardware-specific initial... Show More