Knowledge Base Articles

cancel
Showing results for 
Search instead for 
Did you mean: 
Create an article

Knowledge Base Articles

Recent documents

Sort by:
Chelladurai
Knowledge Base Articles
Version: ** The maximum sense clock frequency [Fsw(max)] is calculated as follows:  The selected sense clock frequency should be such that the senso... Show More
ArunKumarChoul
Knowledge Base Articles
Version: *A PSoC™ 4100S Max, the latest device of the PSoC™ 4 family has additional flash memory, DMA channels, and comes with additional features li... Show More
Chelladurai
Knowledge Base Articles
Version: ** When the CAPSENSE™ shield is enabled, the shield hatch is driven to the same potential as the sensors during the charging and discharging... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Context:The reset status is always set as ‘software reset’ in a bootloadable project for PSoC™ 3/4/5LP MCUs even though the device is res... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** The PSoC™ programmer command-line interface (PPCLI) tool in the PSoC™ programmer installation directory (C:\Program Files (x86)\Cypress\P... Show More
Chelladurai
Knowledge Base Articles
Version: ** Problem: PSoC™ 3 MCU, PSoC™ 4 MCU, PSoC™ 5LP MCU, and some of PSoC™ 6 MCU devices have a powerful and flexible programmable digital perip... Show More
Chelladurai
Knowledge Base Articles
Version: ** Question: What is the workaround for the connection issue between HTerm  and KitProg3 COM port after the KitProg3 firmware update? Answer... Show More
Chelladurai
Knowledge Base Articles
Version: ** The Motorola SPI protocol has four different modes based on how data is driven and captured on the MOSI and MISO lines. These modes are d... Show More
Chelladurai
Knowledge Base Articles
Version: ** This article is for CMSIS5. For information about a previous CMSIS version, see KBA90457. Do the following to include the CMSIS5 Library ... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Question: How can I specify an alternate tools version for my ModusToolbox application? Answer: You can install multiple ModusToolbox sof... Show More