Knowledge Base Articles

cancel
Showing results for 
Search instead for 
Did you mean: 
Create an article

Knowledge Base Articles

Recent documents

Sort by:
Chelladurai
Knowledge Base Articles
Version: ** Is the XENSIVTM PAS CO2 sensor affected by acoustic and vibration noise?XENSIVTM PAS CO2 sensor has a robust packaging, and is acoustica... Show More
Chelladurai
Knowledge Base Articles
Version: ** Watchdog timer (WDT) setting is configured with the following three options when the debugger is connected:   - Counter is stopped when a... Show More
Chelladurai
Knowledge Base Articles
Version: ** ContextDetermine the default setting of the watchdog timer (WDT) at power-on. SolutionTRAVEO™ T2G has two WDTs: basic WDT and multi-count... Show More
Chelladurai
Knowledge Base Articles
Unexpected debugger disconnection during program execution in TRAVEO™ T2G – KBA233857 Version: ** Solution: Check if the following operations are per... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Question: What needs to be checked if JTAG debugger is not connected? Answer: If the signal quality of the hardware is not good, do the f... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Question: How do I evaluate the impact of PLL jitter on CAN precision when PLL clock is used for a CAN peripheral? Answer: Use the follow... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Question: How do I clear the watchdog timer (WDT) in Sleep mode for TRAVEOä II family MCU? Answer: The WDT cannot be cleared in Sleep or ... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Question:What is the thermal resistance for TRAVEOä II CYT2B series? Answer: The thermal parameters (ƟJa, ƟJB, ƟJc) used to characterize ... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Question: Is it possible to use a combination of two different sizes of data fields for buffers/FIFO elements of the CAN FD Controller? ... Show More
ArunKumarChoul
Knowledge Base Articles
Version: ** Question: How can I get the CPU board to operate only at 3.3 V? Answer: Ensure that the jumper settings are as follows: J23: Short bet... Show More