Which HW modules in AURIX™ are capable to generating PWM? – KBA234200
Community Manager
Dec 16, 2021
05:43 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Dec 16, 2021
05:43 AM
Version: **
Both General Timer Module (GTM) and Compare Capture Unit 6 (CCU6x) can generate PWM.
TOM (Timer Output Module) and ATOM (ARU-connected Timer Output Module) in GTM are commonly used to generate PWM; these have the most independent timers and channels to generate PWM in 24-bit resolution (ATOM) or 16-bit resolution (TOM).
Every CCU6x module has two independent timers with 7 channels for PWM generation in 16-bit resolution.
See the “GTM” and “CCU6” sections of the user’s manual for more information.
Note: This KBA applies to the following series of AURIX™ MCUs:
- AURIX™ TC2xx series
- AURIX™ TC3xx series
Labels
Rate this article: