Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Which HW modules in AURIX™ are capable to generating PWM? – KBA234200

Which HW modules in AURIX™ are capable to generating PWM? – KBA234200

IFX_Publisher1
Community Manager
Community Manager
Community Manager
250 sign-ins First comment on KBA 250 replies posted

Version: **

Both General Timer Module (GTM) and Compare Capture Unit 6 (CCU6x) can generate PWM.

TOM (Timer Output Module) and ATOM (ARU-connected Timer Output Module) in GTM are commonly used to generate PWM; these have the most independent timers and channels to generate PWM in 24-bit resolution (ATOM) or 16-bit resolution (TOM).

Every CCU6x module has two independent timers with 7 channels for PWM generation in 16-bit resolution.

See the “GTM” and “CCU6” sections of the user’s manual for more information.

Note: This KBA applies to the following series of AURIX™ MCUs:

  • AURIX™ TC2xx series
  • AURIX™ TC3xx series
0 Likes
355 Views