Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

What programming methods are available for Cypress parallel Flash memory devices? - KBA203736

What programming methods are available for Cypress parallel Flash memory devices? - KBA203736

Anonymous
Not applicable

Version: **

Translation - Japanese: Cypress Parallel Flash Memory が持つプログラミング方法の種類を教えてください - KBA203736 - Community Translated (JA)

Question:

What programming methods are available for Cypress parallel Flash memory devices?

Answer:

There are two programming methods for Cypress parallel Flash memory devices: single-word programming and buffer programming. Please refer to the respective device's datasheet to determine the specific method that the device will support. With either method, a command sequence followed by the address/data to be programmed is required. The Command Definition Table in the datasheet provides the necessary details.

0 Likes
356 Views
Contributors