Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

What is the purpose of BGC100GN6?

What is the purpose of BGC100GN6?

Infineon_Team
Employee
Employee
50 replies posted 25 likes received 25 replies posted

BGC100GN6 is a fully integrated bi-directional coupler IC. It is designed for 2G/3G/4G RF front end applications The device contains a bidirectional coupler operating in one or multiple bands within 0.6 GHz to 2.7 GHz frequency range. The coupled output contains a low-pass filter for 5 GHz ISM blockers suppression. It offers low insertion loss and high directivity. The coupler is controlled via a GPIO pin. This device deploying Infineon high volume RF-CMOS technology. No additional external power supply blocking or RF decoupling capacitors are required. It distinguishes with a very small size of only 1.1 x 0.7mm2 and a maximum height of 0.4 mm.

0 Likes
66 Views