Community Manager

Community Manager
Jun 29, 2022
02:12 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
What is the product description of ITS4075, ITS4040, ITS4090, ITS4130? (KA-01373)
The new PROFET™ family comes with RDSon reaching from 40mΩ to 130mΩ at 2 or 4 switching channels/device respectively
Protection includes low current limit, overheat, loss of ground, over-/under voltage, short circuit
Family members are pin-to-pin compatible along TSDSO14 package
Labels
Rate this article: