Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

What is the difference between the Ready/Busy (RY/BY#) output pin status and the Data Polling (DQ7) method? - KBA203657

What is the difference between the Ready/Busy (RY/BY#) output pin status and the Data Polling (DQ7) method? - KBA203657

Anonymous
Not applicable

Version: **

Translation - Japanese: ステータス確認方法のReady/Busy方式(RY/BY#)とデータポーリング方式(DQ7) の違いを教えてください。- KBA203657 - Community Translated (JA)

Question:

What is the difference between the Ready/Busy (RY/BY#) output pin status and the Data Polling (DQ7) method?

Answer:

The RY/BY# output pin only monitors the current status of the device, and cannot determine if an operation has completed successfully. Since the RY/BY# is an open-drain output pin, it will require the installation of a (4.7K to 10K) pull-up resistor to successfully use this pin. RY/BY# cannot be monitored/accessed via command definitions. The RY/BY# can be left floating if it is not used. The data polling (DQ7) method does not require any conditioning, and will determine if an operation has completed successfully. You may initiate a status read after executing a program or erase command sequence.

0 Likes
1203 Views
Contributors