Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

What happens when the gate voltage VGS exceeds the specified range?

What happens when the gate voltage VGS exceeds the specified range?

Infineon_Team
Employee
Employee
50 replies posted 25 likes received 25 replies posted

The max values in the data sheet (+20 V/-10 V) take into account transient spikes at the gate signal of 5 V max (exceeding the designed gate drive output), which appear no longer than 1% of the total lifetime

– Theoretically, the VGSon could also selected to be a higher value, e.g. 18V, however this will reduce the margin for gate voltage overshoot, which could be challenging for gate drive design and layout.

– Since negative VGSoff for turn-off can have additional impact in the case of CoolSiC™ MOSFETs, Infineon recommends in general to keep the turn-off bias as high as possible, ideally VGSoff = 0 V"

0 Likes
173 Views