Moderator
Jan 23, 2023
01:26 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Jan 23, 2023
01:26 AM
What does the register field TPRECHG - EN_DEEP_AD mean in the datasheet of TLE9210x devices.
Please refer to datasheet of TLE92108-232QX chapter 6.3.3.6.
EN_DEEP_AD means enable deep adaptation. Enabling this deep adaptation feature leads to a lower granularity of the resulting precharge and and predischarge currents.
As is shown in Figure 25 in the datasheet, when EN_DEEP_AD = 1, the pre-charge phase is separated into two sections with two different current. This is called deep adaptation.
This feature can be enabled when a lower granularity of precharge and and predischarge currents is required. In this case, the precharge current is not a constant value, but with two values.
Labels
Rate this article: