Community Manager
Nov 24, 2021
02:28 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Nov 24, 2021
02:28 AM
What does the LITIX™ Basic+ IERRN(fault) parameter stand for?
IERRN(fault) [P_7.5.2], is the strength of the ERRN pin pull-down current, which is minimum 2mA.
During a fault we have to ensure that the pull-down current is stronger than the pull-up current. So, the pull-up current has to be below 2mA.
For more information on the IERRN(fault) parameter and the LITIX™ Basic+ diagnosis check the datasheet and the "LITIX™ Basic+ LED driver family: Diagnosis and fault management" application note
Labels
- Tags:
- LITIX_BASIC+
Rate this article: