Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

What are the protection functions of the PROFET™+ 12V? (KA-01478)

What are the protection functions of the PROFET™+ 12V? (KA-01478)

IFX_Publisher2
Community Manager
Community Manager
Community Manager
1000 replies posted First like given 750 replies posted

Load Dump: 42V Current limitation and secondary protection Thermal shutdown with Restart Enhanced short circuit operation (100k cycles at worst case) (Hardware set-up in accordance to AEC Q100-012 and AEC Q101-006) Loss of ground/battery protection Stable behaviour at under voltage overvoltage protection (ext. components) Voltage dependent current limitation Reverse polarity compliant (ext. components).

0 Likes
81 Views