Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

What are the differences between KP235 and KP235C4115?

What are the differences between KP235 and KP235C4115?

Infineon_Team
Employee
Employee
50 replies posted 25 likes received 25 replies posted

The KP235 and KP235C4115 are different devices with different pressure transfer functions. Therefore, their output is different. Both KP235 & KP235C4115 sensors convert pressure into an analog output signal. The KP235 sensor calibrated transfer function converts a pressure of 40 kPa to 115 kPa into a voltage range of 0.5 V to 4.5 V and the KP235C4115 sensor calibrated transfer function converts a pressure of 15 kPa to 115 kPa into a voltage range of 0.2 V to 4.7 V.

0 Likes
67 Views
Contributors