Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

What are the advantages of using CoolSiC™ MOSFET devices?

What are the advantages of using CoolSiC™ MOSFET devices?

Infineon_Team
Employee
Employee
50 replies posted 25 likes received 25 replies posted

CoolSiC™ MOSFET devices can reduce switching losses by about 80% and conduction losses by up to 50% compared to Si based IGBTs, depending on the load conditions. This leads to a significant reduction in operational costs, since inverter efficiency levels exceeding 99 % can be achieved. Also, CoolSiC™ MOSFET devices reduce system costs by increasing power density.

0 Likes
59 Views