What are the advantages of IR2133 over IR2130?
Community Manager
May 29, 2022
11:43 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
May 29, 2022
11:43 PM
Community Translation: IR2130に対するIR2133の利点は何ですか?(KA-01329)
1. The IR2133 has a shutdown feature -- the SD pin.
2. The deadtime for the IR2133 is shorter.
3. The FLT-CLR pin on the IR2133 allows you to set a lag period between the time the FAULT condition clears, and the time you allow the chip to start functioning normally again.
4. The IR2133 is pin to pin compatible with the 1200V version IR2233.
Labels
- Tags:
- benefits
- design
- driver IC
- gate driver
- Gate Treiber
- IR2130
- IR2133
- Nutzen
- Vorteile
- 栅极驱动器,驱动器IC,优点,Treiber IC
Rate this article: