Version: **
Translation - Japanese: ディープスリープからのPSoC®のウェイクアップ – KBA221487- Community Translated (JA)
Question:
Can the PSoC wake up from a deep sleep on a comparator interrupt?
Answer:
No, the comparator requires a clock to latch in its output to trigger an interrupt. If you can burn two pins, you could run the output of the comparator to the input of a GPIO interrupt and wake up on that.