Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

WICED Enterprise Security Demo

WICED Enterprise Security Demo

GauravS_31
Moderator
Moderator
Moderator
10 questions asked 250 solutions authored 250 sign-ins

This blog post demonstrates how to use Enterprise security protocols in WICED SDK with FreeRADIUS server. This was tested on WICED version Wiced_006.000.001.005, FreeRADIUS version 2.2.9 and ThreadX-NetX_Duo.

 

  1.   Ensure that you have installed freeRADIUS in your Linux PC. Log in to the system as root.
  2.   In the Linux PC, open raddb/users file and create username and password for 802.1X authentication.
  3.   Open raddb/clients.conf and add the IP address of access point which is the RADIUS client for Freeradius and shared secret. This will be used in AP configuration.
  4.   Place your root CA (Certificate Authority) and server certificates along with server private key raddb/certs folder. The same CA shall be used in /libraries/utilities/command_console/wifi/certificate.h.
  5.   Modify the raddb/eap.conf file to include the correct filenames of server private key, server certificate and CA as well as the correct certificate and CA directory. The default certificate directory is raddb/certs.
  6.   Configure the AP to include the radius server IP address and shared secret configured in clients.conf.
  7.   Write the command radiusd -X. If configuration settings are correct, you will see “Ready to process requests” in the end.
  8.   Follow the instructions in the WICED path doc/WICED-Enterprise-Security-User-Guide.pdf to configure your WICED device for enterprise security connection.

  The output would look like

join_ent prints.jpg

 

1170 Views
Comments
AxLi_1746341
Level 7
Level 7
10 comments on KBA 5 comments on KBA First comment on KBA

When will enterprise security work for FreeRTOS build?

GauravS_31
Moderator
Moderator
Moderator
10 questions asked 250 solutions authored 250 sign-ins

I have forwarded your question internally to our development team. I cannot comment on specific date or release.