Employee
Mar 18, 2021
10:46 PM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Mar 18, 2021
10:46 PM
VDDD Power supplied from MiniProg4 in Traveo II Family - KBA232773
Community Translation: Traveo IIファミリのMiniProg4から供給されるVDDD電源 - KBA232773
Version: **
Question:
Is it possible to supply VDDD with MiniProg4?
Answer:
Yes. It is possible to supply VDDD with MiniProg4. However, the maximum output current is approximately 200 mA.
See the “3.3 Power” section of the MiniProg4 Program and Debug Kit Guide for more information
Note: This KBA applies to the following series of Traveo II MCUs:
- CYT2 Series
- CYT3 Series *
- CYT4 Series *
* However, see the datasheet to make sure that the maximum current consumption does not exceed 200 mA.
Labels
Rate this article: