Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

VCC Connection of S6BP201A, S6BP202A, and S6BP203A – KBA225465

VCC Connection of S6BP201A, S6BP202A, and S6BP203A – KBA225465

Community-Team
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Author: jingw_51          Version: **

Translation - Japanese: S6BP201A、S6BP202A、およびS6BP203AのVCC接続 – KBA225465 - Community Translated (JA)

Question: Can the VCC pin of S6BP201A, S6BP202A, and S6BP203A be used to power an external load?

                   

Answer: No. The VCC pin is not for powering external loads. VCC is the LDO output pin of the internal bias voltage. The LDO has no current capability to power external loads. Therefore, do not connect any external load to the VCC pin.

                   

See AN99497 – Designing a Power Management System with S6BP201A, S6BP202A, and S6BP203A for details.

0 Likes
369 Views
Contributors