Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Using“btc_mode” for BT coexistence

Using“btc_mode” for BT coexistence

Infineon_Team
Employee
Employee
50 replies posted 25 likes received 25 replies posted
  1. Default setting for Bluetooth coexistence

In most cases, the Bluetooth coexistence is already implemented by default, and “btc_mode” checks if the Bluetooth coexistence is enabled or not.
The btc_mode parameter can be set in NVRAM as the initial setting, and it is also possible to change the setting by the WL command.

The default value of “btc_mode” depends on the combination of three NVRAM parameters: boardflags”, “boardflags2,  and “btc_mode”.

                   boardflags: bit#0 = 0 or 1
                     (boardflags = 0x00000001)
                   boardflags2: bit#7 = 0 or 1
                     (boardflags2 =0x000000080)
                   btc_mode = 0, 1, or not set


To set the default btc_mode to 1:
 

  1. btc_mode=1 &&  boardflags: bit#0 = 1 && boardflags2:bit#7 = 0
  2. Do not set btc_mode &&  boardflags: bit#0 = 1 && boardflags2:bit#7 = 0


To set the default btc_mode to 0:
 

  1. btc_mode=0 (with any status for boardflags: bit#0 and boardflags2:bit#7)
  2. ! (boardflags: bit#0 = 1 && boardflags2:bit#7 = 0) (with any status for btc_mode or not set)


The “btc_mode” parameter can be set by the WL command to retain the default value.

0 Likes
58 Views
Contributors