Using Port D Pins as GPIO Pins when FX2LP is Configured in Slave FIFO Mode - KBA210880
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Version: *A
Translation - Japanese: FX2LPがスレーブFIFOモードで構成されている場合にポートDピンをGPIOピンとして使用する - KBA210880 - Community Translated (JA)
Question:
How can we use Port D pins as GPIO pins when FX2LP is configured in Slave FIFO mode?
Answer:
The Port D I/O pins of FX2LP can be configured for an alternative function – as the higher 8 bits of the Slave FIFO data bus. For more information, see the FX2LP Technical Reference Manual. To use the Port D pins as GPIO, all the FIFOs should be configured in 8-bit mode. This can be done by setting the WORDWIDE bit (bit 0 in the EPxFIFOCFG registers) as ‘0’. The sequence of commands to configure Port D as a GPIO is as follows.
//Clear all WORDWIDE bits
EP2FIFOCFG = 0x00; SYNCDELAY;
EP4FIFOCFG = 0x00; SYNCDELAY;
EP6FIFOCFG = 0x00; SYNCDELAY;
EP8FIFOCFG = 0x00; SYNCDELAY;
// Set part in Slave FIFO mode
IFCONFIG = 0x43; SYNCDELAY; //set after WORDWIDE bits are cleared
// PORTD can be configured as a GPIO
Note: Ensure that FX2LP is set into Slave FIFO mode only after clearing all the WORDWIDE bits.
-
This widget could not be displayed.Anonymous