Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Using Eclipse IDE for ModusToolbox 2.1 after Installing ModusToolbox 2.2 - KBA231606

Using Eclipse IDE for ModusToolbox 2.1 after Installing ModusToolbox 2.2 - KBA231606

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Version: **

Translation - Japanese: ModusToolbox 2.2をインストール後、ModusToolbox 2.1でEclispe IDEを使用 – KBA231606 - Community Translated (JA)

Question: After installing ModusToolbox 2.2, why am I seeing an error while attempting to program or debug using the Eclipse IDE installed with ModusToolbox 2.1?

error while launching command: [PATH]/ModusToolbox/tools_2.2/CY_TOOL_arm-none-eabi-gdb_EXE --version

Answer: By default, ModusToolbox uses the latest version of the installed tools. In this case, since you have both versions 2.1 and 2.2 installed, the build system is using the 2.2 version of the tools. To resolve this issue, do either of the following:

Option 1: Open the applicable workspace/application using the Eclipse IDE installed with ModusToolbox 2.2.

Option 2: Update the path to the “tools_2.1” directory. Create a CY_TOOLS_PATHS system variable to point to the correct path. For details, refer to the ModusToolbox Installation Guide, section "Create a system variable to specify the path to Tools." Then you can open the application Eclipse IDE installed with ModusToolbox 2.1.

0 Likes
361 Views
Contributors