Using Chip Select Pin as Port Function in Traveo™ S6J3XXX MCUs - KBA223674
Employee
Apr 27, 2018
02:20 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Apr 27, 2018
02:20 AM
Version: **
Translation - Japanese: Traveo™ S6J3XXX MCUのポート機能としてチップセレクトピンを使用 - KBA223674- Community Translated (JA)
Question:
Is it possible to use the chip select pin as a port function when multi-function serial is set to Clock Synchronous Serial Interface (CSIO) mode operation in S6J3110/3120/3200/3300/3350/3360/3370/3400/3510 MCUs?
Answer:
Yes, set the Port Output Function Selection bit (POF) of the Port Setting Register (PPCPCFGR) as a port function for the chip select pin. You can use a chip select pin as a port function and allow the other serial peripheral interface (SPI) pins (SIN/SOUT/SCK) to operate as SPI functions.
Labels
- Tags:
- auto mcu
- chip select
- csio
- mfs
- multi-function serial
- port
- s6j3110
- s6j3120
- s6j3200
- s6j3300
- s6j3350
- s6j3360
- s6j3370
- s6j3400
- s6j3510
- traveo
Rate this article: