Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Using CPU Board at 3.3 V in Traveo II Body Entry - KBA232819

Using CPU Board at 3.3 V in Traveo II Body Entry - KBA232819

ArunKumarChoul
Employee
Employee
50 questions asked 50 sign-ins 25 sign-ins

Version: **

Question:

How can I get the CPU board to operate only at 3.3 V?

Answer:

Ensure that the jumper settings are as follows:

  • J23: Short between pin2 and pin3 (The 3.3 V power rail on the board is enabled).
  • J9: Open between pin1 and pin2 (Power-on-reset for +5 V is disabled).

For more information, see the documentation available with the CYTVII-B-E-1M-176-CPU evaluation board.

Note: This KBA applies to the following series of Traveo II MCUs:

  • Traveo II for Body CYT2B7 Series
0 Likes
315 Views