Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Using CPU Board at 3.3 V in TRAVEO™ II Body Entry (KA-03405)

Using CPU Board at 3.3 V in TRAVEO™ II Body Entry (KA-03405)

MohammedA_41
Community Manager
Community Manager First comment on KBA 250 replies posted First like received
Community Manager

Using CPU Board at 3.3 V in TRAVEO™ II Body Entry (KA-03405)

Ensure that the jumper settings are as follows:

  • J23: Short between pin2 and pin3 (The 3.3 V power rail on the board is enabled).
  • J9: Open between pin1 and pin2 (Power-on-reset for +5 V is disabled).

For more information, see the documentation available with the CYTVII-B-E-1M-176-CPU evaluation board.

Note: This applies to the following series of TRAVEO™ II MCUs:

  • TRAVEO™ II for Body CYT2B7 Series
0 Likes
Contributors