Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Use of the EzI2Cs_bRAM_RWcntr Variable in the EZI2C User Module (UM) - KBA91169

Use of the EzI2Cs_bRAM_RWcntr Variable in the EZI2C User Module (UM) - KBA91169

Anonymous
Not applicable
Version: **

 

Question: What is the use of the EzI2Cs_bRAM_RWcntr variable in the EZI2C UM?

 

Answer:

EzI2Cs_bRAM_RWoffset indicates the start of the offset for the RAM buffer used for EzI2C. EzI2Cs_bRAM_RWcntr is used to keep track of the offset during a read or write operation. It is used as a pointer to indicate the position of the RAM when using EZI2C. EzI2Cs_bRAM_RWcntr is reset to EzI2Cs_bRAM_RWoffset at start of the RW command.

0 Likes
163 Views
Contributors