Usage of CyU3PDeviceGpioRestore in FX3 SDK - KBA233119
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Community Translation: FX3 SDKでのCyU3PDeviceGpioRestoreの使用方法 - KBA233119
Version: **
Question: What is the workaround if we try to override a GPIO that is already overridden?
Answer: In an FX3 device, if we try to override an already overridden GPIO, then it may show erroneous behavior (the GPIO may stay tri-stated).
To avoid this erroneous behavior, the already overridden GPIO should be restored to its normal mode before it is overridden again. For this, the CyU3PDeviceGpioRestore () API can be used. More information on this API can be found in the FX3 API Guide. FX3 API guide comes along with FX3 SDK and can be found in the following path:
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\doc\firmware
The correct sequence of steps to be followed are:
- Invoke the CyU3PDeviceGpioRestore () API for restoring the required GPIO to normal mode.
- Invoke the CyU3PDeviceGpioOverride () API to override the GPIO again.
The above approach can be used if we need to change an already overridden simple GPIO to a complex GPIO or vice versa.