Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Updating an Attribute’s Value in GATT DB of a BLE GATT Server in PSoC 6 BLE – KBA228425

Updating an Attribute’s Value in GATT DB of a BLE GATT Server in PSoC 6 BLE – KBA228425

ChaitanyaV_61
Employee
Employee
50 questions asked 25 likes received 25 sign-ins

Author: GeonaM_26         Version: **

Translation - Japanese: PSoC 6 BLEのBLE GATTサーバのGATT DBの属性値を更新する- KBA228425 - Community Translated (JA)

In a BLE GATT server, the profile-related data are structured in a database called the GATT database. The GATT database consists of the services, characteristics, characteristic descriptors, and declarations present on the server. In PSoC® Creator™, these attributes (characteristics, descriptors) can be initialized in the BLE Component configuration window, under the Profiles tab. If the characteristic value must be updated in run time, the application can do so by using APIs and macros as follows:

  1. When the value must be locally updated by the server itself: A GATT characteristic is often used to reflect a real-time value in an application, such a switch status or a sensor output, which would be read by a GATT Client. To update the value of a characteristic, the application can use the Cy_BLE_GATTS_WriteAttributeValueLocal API function.
  2. When the value must be updated because a GATT Client sent a write request: In this case, use the Cy_BLE_GATTS_WriteAttributeValuePeer () API function.

See the PDL documentation for more details. In PSoC Creator, go to Help > Documentation > Peripheral Driver Library.

0 Likes
687 Views
Contributors